Adding a custom template tab in File --> New

2025-01-06T21:09:28Z

Summary


Details

How can you add a custom template tab in the File --> New dialog of NX? 

Solution

Create a new pax file (you could copy the existing ugs_drawing_templates.pax 

file and rename it) in the %UGII_ROOT_DIR%\templates directory (or you can 

point to custom directory by setting the variable UGII_TEMPLATE_DIR=<path>) 

and store your custom pax file there. Call the file something like <company> 

custom templates.pax

In the pax file, enter the following lines:

<?xml version="1.0" encoding="utf-8"?>

<Palette xmlns="http://www.ugsolutions.com/Schemas/2001/UGPalettes" 

schemaVersion="1.0">

 <Presentation name="Dan's Template (Inch)" bitmap="drawing_new.bmp" 

FileNewTab="Drawing" application="All" UsesMasterModel="Yes"/>

 <PaletteEntry id="d1"> 

 <References/> 

 <Presentation name="Dan's Test Template" description="NX Example, 1 

Sheets"> 

 <PreviewImage type="UGPart" location="drawing_template.jpg"/> 

 </Presentation> 

 <ObjectData class="DrawingTemplate"> 

 <TemplateFileType>none</TemplateFileType> 

 <Filename>Dan's Test Template.prt</Filename> 

 <Units>English</Units> 

 <UsesMasterModel>Yes</UsesMasterModel> 

 </ObjectData> 

 </PaletteEntry>

</Palette>

Change the Presentation Name entry to your custom name:

From: <Presentation name="Drawing Templates (Inch)" bitmap="drawing_new.bmp"

To: <Presentation name="<company custom templates>" bitmap="drawing_new.bmp" 

If you want your drawings on a separate tab, change the the "Drawing" entry of 

the FileNewTab field to your custom tab name in the following:

 <Presentation name="Dan's Template (Inch)" bitmap="drawing_new.bmp" 

FileNewTab="Drawing" application="All" UsesMasterModel="Yes"/>

From: FileNewTab="Drawing" application="All" UsesMasterModel="Yes"/>

To: FileNewTab="<custom name>" application="All" UsesMasterModel="Yes"/>

The following entries are concerning your custom template(s):

<PaletteEntry id="d1"> - (d1 entry must be unique for each template, i.e. d2, 

d3)

<Presentation name="A - Drawing" description="NX Example, 2 Sheets"> - (change 

the Presentation Name to your custome name and modify the description).

<PreviewImage type="UGPart" location="drawing_template.jpg"/> - (change this 

line to point to a jpg of the template. This is optional).

<Filename>A-drawing-template.prt</Filename> - (change to the file name of your 

custom template. This assumes the template file resides in the same directory 

as the pax file. Otherwise, include the path.).

<Units>English</Units> - (change to Metric if necessary).

To add another template, copy the information between <PaletteEntry id="d1"> 

and </PaletteEntry> down to a new section and edit as above.

Make sure the last line in the pax file is </Palette>. 

Save the file and restart NX. The tab should appear in the File --> New 

dialog.

Notes

Notes

KB Article ID# PL8005212

Contents

SummaryDetails

Associated Components