How do we use "Specify component group" option while loading data in NX Manager Mode. Also how do we use it directly from Teamcenter?
Solution
If you are working with "Specify component group" option in Assembly Navigator then you can use the same for loading assembly using "Load Option". After selecting Load as "Specify component group", it will pop up as dialog to select the specific Component Group to be loaded. Refer below snap-



Also, currently there is no way to specify component groups from Teamcenter when loading Assembly by selecting UGMASTER dataset in TC and launching NX to load the same.
Notes and References
9121233
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: FILE_OPEN
Ref: 001-9121233