Where is the 'Find' feature in the new explorer dialog format?

2021-10-06T23:26:24Z

Summary


Details

NX12 is supposed to include a new Find option on operation dialogs. This is not visible in either the default or newer Explorer style dialogs. Where can this be found? 

Solution

This feature is not enabled by default. It must be turned on through a Customer Default option.

  1. Inside an NX session select 'File-->Utilities-->Customer Defaults'.
    1. Expand 'Manufacturing' and highlight 'User Interface'.
      1. Select the 'Dialog Boxes' tab.
        1. Toggle ON the option, "Show Find in Dialog Boxes".
          1. OK the Customer Defaults dialog.
            1. Re-start NX for the change to take effect.

              Notes

              KB Article ID# PL8004876

              Contents

              SummaryDetails

              Associated Components