Problem when inserting a robot model from Siemens into a study; receiving an
error - "Type not defined".
The class type is not defined for downloaded robot models from Siemens. Use
the "Define Component Type" command on the Modeling tab to browse to the
sysroot folder containing the robot model, then set the "Type" of component in
the right-hand column. Now the robot model can be inserted into the study.