NX "Please insert disk1..." when performing an NX Maintenance Release install

2021-10-06T23:26:24Z
NX System Administration

Summary


Details

When performing a Maintenance Release update for NX (updating from NX12 to NX
12.0.2 for example) and the installation kit is on a USB removable drive, the
installation displays the message,

"Please insert disk 1..."

The installation will not continue and must be canceled.


Solution

Copy the installation kit from the USB removable drive to a local hard drive
and re-rin the installation. IT is recommended that you run the NX
installation/update "As Administrator:.


Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: SYSTEM
Version: V12.0.2
Function: WNT_INSTALL

Ref: 001-9228947

KB Article ID# PL8004802

Contents

SummaryDetails

Associated Components

Installation Licensing Plotting