Points in NX12 are bigger compared to NX10

2021-10-06T23:26:24Z

Summary


Details

Datum Points are larger in NX11 and NX12 compared to NX10. 



Solution

In NX11 and NX12, the point object display size can be modified in the Customer Defaults. 
  1. Select 'File-->Utilities-->Customer Defaults'.
  2. Expand 'Gateway' and highlight 'Visualization'.
  3. Select the tab labeled 'Handles/Points'.
  4. Use the drop down menu for the Handle/Point Size setting to select the size (small, medium, large).
    Medium is the default size.
  5. Select OK to close the Dialog.
  6. Restart NX for the Customer Default to take effect. 

Notes and References





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V11.0
Function: CUSTOMER_DEFS

Ref: 001-9222678

KB Article ID# PL8004764

Contents

SummaryDetails

Associated Components