Solid Edge Meaning and use of SEEC_Image_Generate_Asm_3D/SEEC_Image_Generate_3D preferences

2021-10-06T23:52:55Z
DOC_MANAGEMENT

Summary


Details

In the SEEC admin guide there is the following description of the SEEC_Image_Generate_Asm_3D preference: 

"When SEEC_Image_Generate_3D is True and this preference is 1, generate JT files for assembly level geometry. Default is 1." 

However when both preferences are set to 1 (True), nothing happens.  Should not a JT file be generated of all Solid Edge Assemblies (.asm files)?



Solution

There are two preferences controlling JT generation in SEEC:


SEEC_Image_Generate_3D 
SEEC_Image_Generate_Asm_3D


When SEEC_Image_Generate_3D = 1 (True),  JT files are created for parts, sheet metal 
and legacy weldments when uploaded to Teamcenter.


When SEEC_Image_Generate_Asm_3D=1 (True) JT files are generated for assembly level 
geometry like assembly features, frames and weld beads. These JT files are created 
as OVR files (JT override). 


SEEC will not generate JT files for assembly files. 



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219MP10
Function: SEEC

Ref: 001-9220068

KB Article ID# PL8004761

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC