Details
The UGMASTER Dataset not being renamed correctly following a SaveAs
Solution
This can happen if the original Dataset Name does not match the pattern in the
preference UGMASTER_saveas_pattern.
For e.g.
1) Say the Preference value UGMASTER_saveas_pattern is {ItemID}-{RevisionID}
2) For Item/ItemRev 000011/000011/A if the UGMASTER dataset name is 000011
instead of being 000011-A
3) When a user does a SaveAs on 000011/000011/A to 000022/000022/A the dataset
will not be renamed to 000022-A as expected but will remain 000011 because the
original dataset does not match the UGMASTER_saveas_pattern:
{ItemID}-{RevisionID}
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0
Function: FILE_SAVE
Ref: 001-9217175