Siemens PLM Licensing NX: Can't checkout license?

2021-10-06T23:26:23Z
Licensing Maintenance

Summary


Details

Users report that they can't checkout all licenses for NX that should be available; some features in the license file are not at the same version level as others?



Solution

This can happen on sites that have both I-deas and NX on the sold-to. Sometimes the I-deas seats are not bumped to the same revision as NX. Contacting the CAA, which can be found in the top header block of the license file, and asking them to bump I-deas to match NX should resolve this issue. 



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: SYSTEM
Version: V12.0
Function: SYSTEM_TOOLS

Ref: 001-9212876

KB Article ID# PL8004689

Contents

SummaryDetails

Associated Components

Siemens PLM Common Licensing