Receive "Invalid file name" error when attempting to export DXF file

2021-10-06T23:26:23Z

Summary


Details

While attempting to perform an Export DXF/DWG operation, the task could fail with the error "Invalid file name",  especially if you run NX in both managed and native modes on the same computer.


It could be possible that the file path/name has been recorded from managed NX into your dialog memory and thus cause the native session translator to fail when the dialog is being built with the managed path which it cannot not resolve in a native NX session.



Solution

To resolve the issue perform the following:


Menu--> Preferences--> User Interface--> Options--> Dialog Boxes--> Reset Dialog Memory


This should resolve the problem and allow you to access the DXF/DWG translator. 



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: TRANSLATOR
Version: V11.0
Function: DXF_DWG

Ref: 001-9210625

KB Article ID# PL8004674

Contents

SummaryDetails

Associated Components