While launching NX from Teamcenter getting NX Initialization Error. Below is the error-
"Runtime exception in SOA client from of type class UGS::PDM::Model::CDM::User HaTh8cCof1mmd : Type mismatch asking for Char Assay property"
![](/kbassets/PL8004607/7e68e49dcefdee93f3273298cbd9feb8058c0d511005048de6143f4e4418.png)
Solution
Reinstall NX manager to fix the said issue, follow below steps-
1. Remove NX manager integration
2. Remove then NX9 Make sure to delete or rename the entries in the registry from NX9.
HKEY_LOCAL_MACHINE\SOFTWARE\Unigraphics Solutions\NX\9
HKEY_CURRENT_USER\Software\Unigraphics Solutions\NX\9
3. Reinstall NX9 and respective Maintenance Release and Maintenance Patch compatible with your Teamcenter version.
4. Make sure NX is running properly in native mode.
5. Reinstall the NX manager integration
Notes and References
9105179
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V9.0
Function: STARTUP
Ref: 001-9105179