Details
NX Cloning doesn't show up drawing part type in Exceptions list, neither able to clone the Items.
Solution
If the Item Type has mandatory attribute and if it does not have a default value set in BMIDE then clone does not reflect the custom Item types under Default Part Type Exceptions drop down.
So to fix this, set some default value for the mandatory attributes in BMIDE then we can see these Item types as well as we are able to clone them.
Notes and References
9063976
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: NXMANAGER
Function: CLONE
Ref: 001-9063976