Details
Everything works on Robcad V11 except the Teach Pendant.
Error: "FANUC_RJ3_SPOT: Can't get a FLEX license".
Solution
The version of ROBCAD is V11. Check the version of the Fanuc_Rj3_SPOT. ROBCAD doctor will tell you the version of the OLP Controllers. If you see "mp91" in the top left corner, that tells you the version of the controller is 9.1. If ROBCAD is version 11, that is the problem. The two different versions are not compatible.
Uninstall the eM-OLP files with the Control Panel ->Programs ->Programs and features.
In the registry, delete the folder "mp91". Here is the location: HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Tecnomatix\eM_OLP\mp91
Notes and References
It is not recommended that you use either the uninstall feature in the control panel, or the registry editor (regedit) if you are not familiar with them. Removing the wrong files or data can be disastrous.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: ROBCAD
Version: V11.0R
Function: ROBCAD_GENERAL
Ref: 001-9040272