How to change member of alternate position of assembly on the same drawing view?

2021-10-06T23:52:45Z

Summary


Details

After creating alternate position of assembly and placing drawing view of one member on Draft Sheet.
Now we want to show the alternate position (another member) on the same view?

Solution

Use the Set Primary and Alternate Positions dialog box to show or hide assembly members in a selected alternate position assembly drawing view. If you change the member selections, you must update the view.
 
This dialog box is displayed when you select the Set Primary and Alternate Positions command from the shortcut menu of an alternate position assembly drawing view. 
 
Steps:
1. Open the drawing having drawing view of Alternate assembly member.
2. Select the view > RMB (Right mouse button) click > Select 'Set Primary and Alternate Positions'
3. Check select the Member (which user wish to have drawing view placed in the drawing) as primary and deselect any check mark in Alternate column.
4. Update the drawing view.
This will define the selected member as Primary member for particular drawing view.

Notes and References

8549152

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: DRAWING_VIEWS

Ref: 001-8549152

KB Article ID# PL8004587

Contents

SummaryDetails

Associated Components