Regenerate does not reduce facet size when zoom in like previous NX8 release.

2021-10-06T23:26:22Z

Summary


Details

Regenerate Functions Differently in NX9 and LaterVersus Earlier NX Releases. 



Solution

When working with shaded displays in Modeling Application NX added display 
facet caching in NX9.


Prior to NX9, when a regeneration request for a solid was made, NX had to 
tessellate the solid, which could be very time intensive.


Starting in NX9 when a regeneration request is done on a solid, and NX has 
available and up to date facets in the facet cache, NX uses those (no 
tessellation occurs).  This introduces significant time savings on a 
regeneration in general.  The other thing NX now does is change the default 
—facet scaling™ factor from view-based to part-based scaling.  This last change 
can have a noticeable impact when zoomed in significantly on a model (besides 
the faster aspect, it can be a little cruder than view-based scaling, 
especially as you zoom in).  The main reason this was changed to the 
facet-scaling factor is that it allows facets to be reused much more often.


One consequence of changing facet scaling was that it became noticeable that 
NX did not always explicitly specify a chordal angular tolerance when 
generating facets - this was a holdover from earlier option specifications for 
using the Parasolid tessellated for NX display.  View-based facet scaling hid 
the fact that not specifying the angular tolerance could result in poor 
looking circles (for example holes) in general.  When a part is —fit™ in the view, 
the view scale and the part box scale are similar (usually) so the results are 
generally the same there, so it is also generally not as noticeable there.


NX12 will always attempt to specify an explicit chordal angular tolerance - 
this improves display quality in general, especially around curved edges.


When introducing facet caching, we decided to leave Update Display as a 
means to quickly improve the facet quality,  as though View-based 
facet scaling was in effect, without the need to go to a dialog that exposes 
facet settings.  However, those changes are generally transient, in that if a 
subsequent regeneration is made, we opt for the settings in effect (which 
generally results in fewer facets when part-based facet scaling is in effect). 

NX should now use  the most precise set of facets that NX has available,
(if a complete set is available at that precision), on subsequent regeneration 
requests (also in NX12).



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: SYSENG
Version: V11.0.1
Function: DISPLAY

Ref: 001-9198248

KB Article ID# PL8004577

Contents

SummaryDetails

Associated Components