MCD Objects created from a Source cannot be grabbed except for the first object

2021-10-06T23:26:22Z

Summary


Details

Objects created from a Source cannot be grabbed (selected) during simulation
except for the first object.


Solution

NX 12.0.2 does solve this issue.

What actually happens in NX 12.0.1 is that a background object is selected
instead of the (moving) SourceObject, and no Quick-Pick will appear.

3 possible workarounds to overcome this behavior:

1) Rotate your model so there is no other object to select (behind the target);
2) Set selection filter to "Facet Body" during simulation;
3) Make the layer of the background-objects Visible Only.
The source object will appear at the work layer and be selectable.


Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1507
Product: NX
Application: MECHATRONICS
Version: V12.0.1
Function: RUN_TIME

Ref: 001-9204355

KB Article ID# PL8004569

Contents

SummaryDetails

Associated Components