NX Edge names are not removed from WAVE link body

2021-10-06T23:26:22Z
NX for Design

Summary


Details

We have a solid object, where several edges have specific Names.
I.e. we selected Edge, opened "Properties\General\Feature Name" and set custom
name for the Edge.
After this we created associative WAVE link from this solid object.
And now we try to delete all custom Edges Names in the link.

We can delete it in the link, save the link, but after reopen it custom Edges
Names still exist.


Solution

For all NX version:

If we create associative WAVE link from geometry feature, all attributes of
this feature are passed to the link. E.g. Material, feature Names.
It works as designed.

We can delete such attributes only from non-associative WAVE link.

References: PR_7953583, PR_7913179.

Developer explanation:

Many things are automatically inherited when WAVE linking a body (regardless
of settings, e.g. Object Names, Attributes, Materials).
All of these inherited Name and Material behaviors seems like reasonable
assumptions.


Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V10.0.3
Function: WAVE

Ref: 001-9193299

KB Article ID# PL8004539

Contents

SummaryDetails

Associated Components

Assemblies