Details
When re-importing a package file with ATT, ATTI, what is the effect if there is no Manifest file?
Solution
Manifest file will get create while downloading SE files through SEEC cache assistance (create package).
Manifest file will have some information like properties, UID, meta model information etc. so it is mandatory/recommended when reimporting using ATTI.
Manifest file is not required when using ATT.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110.0
Function: SEEC
Ref: 001-9200203