NX Unable to delete the feature name in wave geometry body.

2019-08-27T09:39:45Z
NX for Design

Summary


Details

Unable to delete the feature name in wave geometry body when the original solid body is hidden.

Solution

Inheriting the name from the source is designed behavior. 


The name can be edited, but if the user name is deleted the system name inherited from its source body is restored. 

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V12.0.1
Function: WAVE

Ref: 001-9176891

KB Article ID# PL8004524

Contents

SummaryDetails

Associated Components

Assemblies