Details
Making a component the Displayed Part and performing an Assemblies Where Used
report does not report any results.
Solution
This will occur if the component has Reference-Only toggled in ON.
If a component is declared as reference only it means that it does not belong
to the BOM line but it is used to facilitate the establishment of the assembly
in the NX environment. Therefore, during save of the assembly back to TC, the
reference component is removed from the BOM line as if it is not part of the
assembly.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V4.0.3
Function: ASSEMBLY
Ref: 001-9198692