Details
Download machinery library tool
Double click MachineryLibrary-installation.bat file, Select Teamcenter mode
Select new installation
Download GBXXX.zip from GTAC
Place it in the machinery library tool lib folder
Then the installation will recognize the gb standard parts.
Once the import is finished , you can see in TC , only the family template is created, no family members are created.
Solution
Its working as designed.
Only part family templates will be imported , no family members will be created while importing
You have to generate it manually from NX from spreadsheet
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: KDA
Version: V11.0
Function: REUSE_LIBRARY
Ref: 001-9180369