Details
NX Manager Export Assembly or ugmanager_clone on an assembly drawing that contains a pattern file reference will not translate the pattern file to the native file name format.
Solution
Ugmanager_clone does not translate pattern file names when we do both import and export. So in this case the TC database part name will still be in the OS part file once it is exported. This is by design.
Customers must either use ug_export/ug_import. The other option is to keep all pattern files at the OS level and use UGII_PATDIR to point the directory that contains all pattern files.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V8.5.3
Function: CLONE_EXPORT
Ref: 001-9160462