Revision Rules for reuse library not found in NX12

2021-10-06T23:26:22Z

Summary


Details

In NX 8.5 customer default Revision Rule for Precise Only can be set with "Precise Only", "Precise Only (latest Released)" but the same setting is not available in NX 12.

Solution

In NX versions prior to NX8.5.3 reuse library components were loaded using the overall assembly load option setting for which revision rule to use.
  
  In NX8.5.3 the NX customer default "Use 'Last Released' Revision Rule in Reuse Library" was introduced as an on/off toggle.
  In addition another setting was introduced in NX8.5.2, "Revision Rule for Precise Only" with the 3 options:
              Last Modified(default)/Last Released/Asking to Select
  Both these settings are found in NX customer default under Gateway -> Reuse Library, General tab.
  
  In NX10 the above mentioned NX customer default setting were replaced by a different approach. Reuse Library have its own revision rule (MB 3 on header area of Reuse Library navigator). So any revision rule available can be used and if necessary a need special revision rule for Reuse Library can be created in TC. 

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.1
Function: PREFERENCES

Ref: 001-9178069

KB Article ID# PL8004493

Contents

SummaryDetails

Associated Components