How to recognize components when Part Handle (PH) numbers are shown in ANT?

2024-09-23T06:42:05Z

Summary


Details

How to recognize components when PH numbers are shown in ANT? 


This happens when parts are exported from TC from the named reference of a dataset or PLMXLM-export, and left unloaded. 

Solution

As help to recognize the components, you can use the attributes DB_PART_NO and DB_PART_REV to add as new columns to the assembly navigator.


Exported an assembly from TC-database to PLMXML is meant to be imported into another TC-database. When the NX assembly has to be opened in a native NX session, then you best use command Export Assembly from Teamcenter in NXmanager (NX in managed mode which is connected to TC). 

Notes

Notes

KB Article ID# PL8004481

Contents

SummaryDetails

Associated Components