Solid Edge Changing user defined quantity does not change mass.

2021-10-06T23:52:38Z
ASSEMBLY

Summary


Details

Changing user defined quantity does not change mass.

Solution

There are two fields regarding Mass in the Physical Properties command. One is 
for the mass of the assembly (Mass field) without overrides and the other is 
for the mass of the assembly with any overrides (Quantity Override Mass field). 
So the Mass field contains the mass value for the assembly without any 
overrides. When overrides do exist, the Quantity override mass field contains 
the mass value for the assembly taking the overrides in consideration. This is 
easy to overlook at times. 



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V109MP11
Function: TOOLS

Ref: 001-9194989

KB Article ID# PL8004465

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS