NX Added a spring pass to countersink and only get 1 pass

2021-10-06T23:26:21Z
NX for Manufacturing

Summary


Details

Hole Milling and Countersinking operation needs a spring pass.

Solution

In the new hole milling operation, under the non-cutting-moves dialog, there is 

an option called 'Overlap'. This option will allow the user to countersink more than 1 pass 

to make sure the cut is clean.

 Say the user wanted to cut twice (with a spring pass), the overlap option can be set to 'Angle' and the 'Angle' option set to 360 degrees.  This will produce the spring pass. 

Notes

KB Article ID# PL8004440

Contents

SummaryDetails

Associated Components

Manufacturing General