Details
Want to export the company logo in the title block (and images in the drawing).
Solution
Up to NX10 a drawing which includes the company LOGO and/or an embedded image,
the Logo/image is not exported when exporting this drawing to DXF/DWG.
With NX11 export to DXF/DWG does include the Logo/image.
The result is not only a DXF/DWG file but also separate JPEG file(s) are created,
one for each Logo/image.
There's no option to avoid this, since AutoCAD does not include the picture within the drawing, it just creates a link to its location.
Keep in mind that Shaded views are NOT exported as Shaded !
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: TRANSLATOR
Version: V11.0
Function: DXF_DWG
Ref: 001-9041060