Line widths appear thinner when printing in NX11.0

2021-10-06T23:26:21Z

Summary


Details

Line widths appear thinner when printing in NX11.0.

Solution

The customer defaults for the print width scale factors changed in NX10.0 and later versions.  
The print width scale factors for NX8.5 thru NX9.0 are:  1, 2, 3, 4, 5, 6, 7, 8, 9
In NX10.0 and later versions, the print width scale factors are:  1, 1, 1, 1, 2, 2, 3, 3, 3
 
 Here's how to change the Customer Defaults for the print width scale factors: 
1.  Select 'File-->Utilities-->Customer Defaults '. 
2.  Expand 'Gateway', and highlight 'Printing (Windows Only)'.
3.  Under the 'General' tab, assign Width 1 Scale Factor through Width 9 Scale Factor the values of: 
      1, 2, 3, 4, 5, 6, 7, 8, 9
4.  OK the Customer Defaults dialog and restart NX for the settings to take effect.
 
After NX has been restarted, the dialog Print memory should be reset.  This can be done in the Print dialog box (circular arrow next to the 'X' in the top right hand corner of the dialog). 
Or go to 'File-->Preferences-->User Interface' and select 'Option'. Then select the 'Reset Dialog Memory' icon in the Dialog Boxes group.

Notes and References





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V11.0
Function: CUSTOMER_DEFS

Ref: 001-9187466

KB Article ID# PL8004429

Contents

SummaryDetails

Associated Components