SEEC is unable to log in when using TCCS.

2021-10-06T23:52:36Z

Summary


Details

SEEC is unable to sign in to Teamcenter when configured for Teamcenter Client Communication. 

Solution

The error encountered is 'No Teamcenter environments are defined. Use Teamcenter 
Environment Manage to configure a Teamcenter client communication system (TCCS) environment. Refresh your list of available environments in Solid Edge Options - Manage'.


Go to 'Solid Edge Options -> Manage -> Create or update the list of Teamcenter environments' (button with the Teamcenter icon just above 'Go Offline'). Check the 'Activate' box at the bottom of the 'Define Teamcenter Environments' dialog, select the URL with TCCS=yes and SSO=yes, click 'Update' and click OK. Login should then succeed.

Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP6
Function: SEEC

Ref: 001-9187428

KB Article ID# PL8004421

Contents

SummaryDetails

Associated Components