Details
Since 4K monitors and newest version of NVIDIA driver have been installed, Process Simulate will not launch. The type of NVIDIA hardware is Quadro M1000M. The resolution is set to 3840 x 2160 (4K equivalent).
Solution
Use an older NVIDIA driver; version 376.99 will let Process Simulate launch, and monitors will be capable of 3840 x 2160 resolution (4K equivalent).
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANNING_APPLIC
Version: V14.0
Function: PROCESS_SIMULAT
Ref: 001-9183458