Simcenter 3D Solutions How can I change a load set or constraint set id?

2021-10-06T23:26:20Z
Simcenter 3D

Summary


Details

Can I define the load set id or constraint set id that will be exported to a Simcenter Nastran input file?

Solution

Load and constraint set id's can be assigned when a solver set is used to include the sets in a solution, 

but id's can not be assigned or changed for loads or constraints in the load container or constraint container.

Notes

KB Article ID# PL8004346

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow