Not able to search specific properties on one computer

2021-10-06T23:52:32Z

Summary


Details

Using Solid Edge data management with a Fast Search server we, unable to 
search custom properties. 



Solution

The custom properties on the Fast Search server and the Solid Edge clients 
must match exactly as per the SEUser.propdesc. To ensure they match follow 
these steps:


- place the propseed.txt on a shared network location and set the file location 
 on the Fast Search server and Solid Edge clients. 
- on the Fast Search server set custom properties using the propseed only 
** DO NOT use the option for templates. 
- rebuild index on the server


- on the client set custom properties using the SAME propseed only 
** DO NOT use the option for templates. 
- rebuild index 
- restart Explorer.exe or reboot



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110.0
Function: BUILT_IN

Ref: 001-9141002

KB Article ID# PL8004340

Contents

SummaryDetails

Associated Components