Quantity with decimal does not reflect in the parts list

2021-10-06T23:26:20Z

Summary


Details

1) create an item in TC using the Custom UOM
2) Create an Assembly in NX 
3) Add (1) to the Assembly created in Step 2
4) change the quantity to 1.1 
5) Go to the drafting and generate the parts list, It shown the quantity as 1 instead of 1.1

Solution

o Right click on the Parts list - > select Cell settings
o Common - Cell - Under Format Decimal Places enter 2
 
 This should help to display 2 decimal places values in the cells instead of rounding the values.

Notes and References

IR 9148190 

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V9.0.3
Function: TABLES

Ref: 001-9148190

KB Article ID# PL8004299

Contents

SummaryDetails

Associated Components