Solid Edge Text is faint when creating pdf.

2021-10-06T23:52:31Z
DRAFT

Summary


Details

Text is faint when creating pdf. 



Solution

This can happen if the text in the table style is set to Monotxt. Even though the 'Save all colors as black' is selected in the PDF Export Options, the text is still dithered. The solution is to uninstall the Monotxt font and let Solid Edge pick the default. 



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: DRAFT
Version: V110MP5
Function: FILE

Ref: 001-9167039

KB Article ID# PL8004296

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS