Details
When using EditWithUnits and trying to pass in a variable for a string expression you may receive a datatype error.
Dim xyz As String = "123456"
workPart.Expressions.EditWithUnits(expression1, nullUnit, xyz)
Solution
This will happen because NX expects to receive a string value for the input.
Although XYZ in this case -
Dim xyz As String = "123456"
workPart.Expressions.EditWithUnits(expression1, nullUnit, xyz)
- is defined as a string, NX interprets it as an integer. To correct the issue, escape the double-quote (") character and include it in the value:
Dim xyz As String = """123456""" \\ for VB
workPart.Expressions.EditWithUnits(expression1, nullUnit, xyz)
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: SYSENG
Version: V8.0
Function: NXOPEN
Ref: 001-9164748