Details
How do users activate the Help button for Moldwizard Standard Parts?
Solution
Users need to open the spreadsheet of the slide or lifter for example, and add keyword HELP in
the excel data file. For example.
HELP ../help/MC Table of Contents.pdf
where "HELP" is in the first cell, and the path and file name are in the second cell.
The value of HELP (second cell) can be a file of type txt, word, pptx, pdf, image, web address, html link, avi, etc. Make sure the file path you provide is valid.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 1064
Product: NX
Application: KDA
Version: V11.0
Function: MOLDWIZARD
Ref: 001-9153971