Part Physical Properties will not update

2021-10-06T23:52:26Z

Summary


Details

Physical Properties do not update in a part file. 



Solution

One of the common reasons for this is that Maintain Relationships is turned off in the file. To check, go to Tools tab and click the Update Active Level pulldown, check the Automatic Update icon: it should be selected. The icon should have a light blue background. If not, click on it to turn it on. That should allow the Physical Properties to work correctly again. It is recommended that Automatic Update is kept on at all times. This option is stored with the file and is NOT a user preference.



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V109MP14
Function: UPDATE

Ref: 001-9154866

KB Article ID# PL8004225

Contents

SummaryDetails

Associated Components