When importing a JT file that contains an assembly into Solid Edge Part it may appear that after import the geometry is not one single Body, but consists of a lot of Construction Bodies instead when what was expected was a single Design Body.
Solution
If you need to have a single Design Body later on, then while initially exporting the Body to JT in a single JT-file you need to set the option:
"Include precise geometry = ON"
This will then result in a single Design Body when importing the JT file back into Solid Edge Part.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V110MP7
Function: JT
Ref: 001-9094821