Symptom
=======
Can I combine multiple license files together into one license file/license
server?
Solution
========
Even though it is technically possible to combine license files for the same
product, in some special instances, it is not supported by Siemens PLM. The
process is very specific, and customized.
All of the licenses need to be created for the same license server with the
same CID.
If there are duplicate FEATURES in the license file, the one with the newest
CREATION DATE takes priority.
To make sure that duplicate features will be cumulated, the licenses which
will be merged must have the same creation date.