Disconnecting Tabular Note from Spreadsheet

2021-10-06T23:26:19Z

Summary


Details

When creating/editing a Tabular note using a large amount of data in
spreadsheet, the updates will take a long time. This is due to the COM
between Excel and NX through shared Windows O/S abilities. After getting the
initial data imported, the spreadsheet edit may no longer be wanted and you
might want to disconnect the Tabular Note from Spreadsheet.


Solution

Select the Tabular Note upper left corner where the "+" is, then with MB3 ->
Edit without using Spreadsheet. There will be a warning to acknowledge, and
once done the Tabular Note can be edited as a simple Tabular Note.


Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: redhat
OS Version: EL6.0
Product: NX
Application: DRAFTING
Version: V10.0.3
Function: TABLES

Ref: 001-9150319

KB Article ID# PL8004180

Contents

SummaryDetails

Associated Components