Solid Edge Linking variables in Solid Edge to Excel hosted on a Citrix server

2021-10-06T23:52:17Z
PART/SHEETMETAL

Summary


Details

Solid Edge is installed on the local client but the Microsoft Excel application is installed on a Citirx server.  Can Solid Edge variables still be linked to Excel?

Solution

Solid Edge expects Excel to be installed locally to the same client as where Solid Edge is installed. 

If Excel is hosted or installed on a Citrix server, then Excel is *not* local to the Solid Edge installation.  Therefore it would not be possible to link Solid Edge variables to Excel in this configuration.  

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V110.0
Function: OLE

Ref: 001-7952259

KB Article ID# PL8004166

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN