- Display result with overflow (post view1)
- Post view settings\Legend:
Set a Color Bar Max value
Activate overflow on
- Display the Max annotation value
In SimCenter 12 the maximum annotation is below the overflow (it was not
filtered in Simcenter 11 and before, max value was above overflow)
Solution
If you need to display the max annotation value for all results (above
overflow limit):
- Select the same result and overlay to the display: It will create a post
view2
- Edit the post view 2
- Display tab:
Deactivate the color Display and set Faces to "no Fill"
- Display the max annotation value
- Make post view 1 active to display the color bar of post view1
You will see in the same display the result with max annotation value under
and above overflow using the color bar of overflow.
Notes