Simcenter 3D Solutions Is It Possible to Export Groups for ABAQUS Even If They're Not Used?

2021-10-06T23:26:19Z
Simcenter 3D

Summary


Details

A Customer was running NX11.0.X, using Pre/Post, and doing ABAQUS axisymmetric structural.

He asked the question above.

Solution

Yes groups can be exported even if they are not used.

If you click on Solution -> Edit Solver Parameters, then activate "Write out group data", then the groups will be written to the deck. 

Notes

IR 9110181.

KB Article ID# PL8004156

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow