Is there a preference or setting to enable Inspect -> Relationships Color to be turned on by default?
Solution
Currently there is no UI interface to enable Inspect -> Relationships Color to be turned on by default.
However, you can enable Inspect -> Relationships Color to be turned on through the user's registry settings. The following combination of registry keys will turn on Inspect -> Relationships Color:
[HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 110\PrefSets\Options-Color]
"ColorByDOF"=hex:06,00,00,00,00,00,00,00,01,00,00,00,00,00,00,00
[HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 110\Part\Preferences\Options-Color]
"ColorByDOF"=hex:06,00,00,00,00,00,00,00,01,00,00,00,00,00,00,00
"SKColorByDOF"=hex:06,00,00,00,00,00,00,00,01,00,00,00,00,00,00,00Please note that setting Solid Edge user preferences through the registry is not supported by GTAC.
Notes and References
See the following Solid Edge documentation for more on Relationship Colors:
https://docs.plm.automation.siemens.com/tdoc/se/110/se_help/#uid:index#goto:user_interface:skchrlshpcolor1cHardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V110.0
Function: OTHER
Ref: 001-8364912