Is there a way to place a "Center of Mass" type symbol in Draft?

2021-10-06T23:52:09Z

Summary


Details

Is there a way to place a "Center of Mass" type symbol in Draft? 



Solution

Yes! When in a Draft file, if you go to the Library tab of EdgeBar and make 
sure the Show Blocks button is pushed in (first button at the top of the tab 
under the tabs themselves). Now go to the lower pane of the EdgeBar and there 
should be a list of documents or it may just say "Active Document". Click on 
the plus sign in front of the Active Document (if it is not already expanded) 
and you should see an item "COM". This is a block and you you can drag it 
into the graphics window and your next click will place it. 



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: DRAFT
Version: V109MP12
Function: ANNOTATIONS

Ref: 001-9147445

KB Article ID# PL8004127

Contents

SummaryDetails

Associated Components