Unable to get Material to map to the UGPART-ATTR form in the Named References

2021-10-06T23:26:19Z

Summary


Details

How to get Material attribute to map to the UGPART-ATTR form in the Named References of UGMaster dataset?

Solution

Use the following set up steps in NX11: 
(1) Customer Defaults > Gateway > Material/Mass > Attributes tab: 
Part Material 
Attribute Title Alias = Material 
(2) In Attr mapping file: 
{ Dataset type="UGMASTER" 
 NX_Material:NR( UGPART-ATTR ).material /master=cad /description=™Material 
on UGPART-ATTR form™ 
(3) Create a new item in NX with a solid block, assign material to the block 
(4) Save in NX 
(5) In Teamcenter bring up Named References form on UGMaster dataset. 
(6) Highlight the row "UGPART-ATTR" and Open 
(7) In the UGPART-ATTR form, the Material field shows the name of material 
assigned from step(3).


Note: the key for this to function is to make sure the attribute mapping file 
is using the updated syntax that is documented specifically for NX11. 
Documenatation location is here: 
Doc Center > Home > Teamcenter Integration for NX > Attributes > Mapping 
Attributes > Example Layout of a Mapping File 

Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 2012_R2
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: ATTRIBUTES

Ref: 001-9145017

KB Article ID# PL8004110

Contents

SummaryDetails

Associated Components