Simcenter 3D Solutions Bounding volume based mesh controls not working with selection recipes

2021-10-06T23:26:19Z
Simcenter 3D

Summary


Details

I have created a bounding volume selection recipe and used the recipe when creating a bounding volume mesh control. Why is this mesh control not working?

Solution

When creating a bounding volume mesh control, a recipe must be selected. A polygon body can optionally be selected. To control a mesh defined using polygon bodies or faces, such as 3d tetrahedral mesh, a body must also be selected, even though the form allows Apply or OK without selecting any body.

For mesh definitions that don't rely on polygon geometry, such as 3d hybrid meshes or solid from shell meshes, only the recipe selection is required.


Image1.jpg 18.34 KB

Notes


Image1.jpg 18.34 KB

KB Article ID# PL8004062

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow