Additive Manufacturing : Are there any EOS machine templates available for NX?
Solution
At the moment, we just have the TRUMPF templates listed, but it can easily be
modified to include additional machine definitions:
edit NX\MACH\templates\ugs_additive_manufacuring_templates.pax :
- Copy one of the printer entries:
<PaletteEntry id="d3">
<References/>
<Presentation name="TRUMPF TruPrint 1000" description="NX Additive
Manufacturing Part for TRUMPF TruPrint 1000">
<PreviewImage type="UGPart" location="TRUMPF_TruPrint_1000.jpg"/>
</Presentation>
<ObjectData class="AdditiveManufacturingTemplate">
<Filename>trumpf_truprint1000-mm-part-template.prt</Filename>
<Units>Metric</Units>
<UsesMasterModel>No</UsesMasterModel>
</ObjectData>
</PaletteEntry>
- then paste and edit this section, making reference to the EOS template part
and jpg
<PaletteEntry id="d7">
<References/>
<Presentation name="EOS" description="NX Additive Manufacturing Part
for EOS">
<PreviewImage type="UGPart" location="EOS.jpg"/>
</Presentation>
<ObjectData class="AdditiveManufacturingTemplate">
<Filename>EOS.prt</Filename>
<Units>Metric</Units>
<UsesMasterModel>No</UsesMasterModel>
</ObjectData>
</PaletteEntry>
The EOS-mm-part-template.prt would need to be created in NX\MACH\templates ,
but could be based on an existing part file eg
trumpf_truprint1000-mm-part-template.prt
In a similar way, a jpg of the machine needs creating in the same folder.
Notes