NX Fatal error switching to Manufacturing application

2021-10-06T23:26:18Z
NX for Manufacturing

Summary


Details

Part files from NX10 will open fine in Gateway or Modeling, but then NX issues an error when trying to switch to the Manufacturing application. The software crashes out to Gateway. The same happens when creating a new part file in NX12 and trying to switch to the Manufacturing application.

Solution

Check the NX syslog file for details on the error conditions. In this case, the log file records:

APP_EXITED_APPLICATION_ENVIRONMENT_CALLBACK_ID UG_APP_GATEWAY. 

*** NOTE:: in line 1596 of 

o:\ugnx120\ip27\src\cams\no\ind\cam_session_definitions.c at Fri Apr 13 

08:51:34 2018 Central Daylight Time 

+++ An invalid key word FEATURE_RECOGNITION in file 

C:\Program Files\Siemens\NX 12.0\mach\resource\configuration\cam_general.dat 

MB_LOADED_MENU_FILE Successfully loaded menu file: C:\Program Files\Siemens\NX 

12.0\mach\application\ug_cam.men 

MB_LOADED_MENU_FILE Successfully loaded menu file: C:\Program Files\Siemens\NX 

12.0\ugii\menus\ug_synchronous.men 

MB_LOADED_MENU_FILE Successfully loaded menu file: C:\Program Files\Siemens\NX 

12.0\mach\application\ug_cam_view_popup.men 

Successfully loaded dynamic module C:\Program Files\Siemens\NX 

12.0\NXBIN\libtcl.dll 

Loaded module c:\program files\siemens\nx 12.0\nxbin\libtcl.dll 162b0000 a1000 

0-0-0-0-0 version = 8.4.2.19 

Successfully loaded dynamic module C:\Program Files\Siemens\NX 

12.0\NXBIN\libcamsja.dll 

Loaded module c:\program files\siemens\nx 12.0\nxbin\libcamsja.dll 

7ffad1580000 997000 

d44434f0-453b75c9-f0e2d79d-fb8e2de1-1=libcamsja___1506521580cyp version = 

12.0.0.27 

*** EXCEPTION: Error code 1990056 in line 837 of 

o:\ugnx120\ip27\src\cams\no\ind\cam_session_definitions.c at Fri Apr 13 

08:51:35 2018 Central Daylight Time 

+++ The FEATURE_RECOGNITION keyword is obsolete and should be removed from the 

configuration file.

 followed by tracebacks and then 

>>>> Error code 1990056 caught in file 

"o:\ugnx120\ip27\drv\camsja\no\ind\ja_cam_camsession_jam.cxx" at line number 

100 

>>>> Error code 1990056 caught in file 

"o:\ugnx120\ip27\src\ugui\no\ind\ui_app.c" at line number 2314 

>>>> Error code 1990056 successfully handled and acknowledged 

*** EXCEPTION: O/S ERROR: signal 11 in line 2602 of 

o:\ugnx120\ip27\src\syss\error\ind\error.cxx at Fri Apr 13 08:51:36 2018 

Central Daylight Time 

+++ General Fault Exception 

+++ Invalid read from 0000000000000000 

 rsp: 5f33f0, rip: 7ffad4a08fcd, rbp: 5f38d0 

 rsi: 5f3e90, rdi: 0 

 rax: 0, rbx: 16020090, rcx: 0, rdx: 

 0 

 r8: 5, r9: 6500, r10: 7ffafc432a20, r11: 

 7ff5fc5ecbc8 

 r12: 5f3e90, r13: 5f3ac0, r14: 0, r15: 

 0

A check of the named cam_general.dat configuration file shows that it does contain a line item entry named "FEATURE_RECOGNITION." Removing this line from the configuration file satisfies the NX12 launch criteria and the session can be changed to the Manufacturing application without error.

Notes

KB Article ID# PL8004037

Contents

SummaryDetails

Associated Components

Manufacturing General