NX Not all license bundles are available in the NX Licensing Tool with mulitple REDUNDANT servers

2021-10-06T23:26:18Z
NX System Administration

Summary


Details

Not all license bundles are available in the NX Licensing Tool when multiple REDUNDANT license servers are defined.



Solution

The user has two different REDUNDANT license servers. The value of SPLM_LICENSE_SERVER is 


SPLM_LICENSE_SERVER=28000@server1,28000@server2,28000@server3,28000@server4,280 
00@server5,28000@server6


The delimiter for REDUNDANT license servers is a comma (,) but in this instance, the user 
has TWO redundant server configurations. 

The delmiter for MULTIPLE license servers is a semi-colon (;). The user needs to change the delimiter BETWEEN the two recundant servers to a semi-colon. For example,


SPLM_LICENSE_SERVER=28000@server1,28000@server2,28000@server3;28000@server4,280 
00@server5,28000@server6

(Note the semi-colon between 'server3' and 'server4'.


Once the semi-colon (;) is added between the two sets of REDUNDANT license servers, the NX end-users should be able see all of the available license bundles.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: SYSTEM
Version: V12.0
Function: WNT_OS_ISSUES

Ref: 001-9133311

KB Article ID# PL8004034

Contents

SummaryDetails

Associated Components

Installation